AXIS#.OBS.ENABLE

Description

AXIS#.OBS.ENABLE turns the Observer on and off. When the Observer is in the disabled state (0), it passes the raw velocity feedback into the control loops.


  • This setting cannot be changed while the amplifier is enabled in order to minimize unexpected disturbances.

The Observer is made up of a few components. Following is a block diagram of how the Observer is connected in the loops.

Versions

Action Version Notes
Implemented 02-04-03-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.OBS.ENABLE

5017h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.OBS.ENABLE

5117h

02h

Unsigned8

-

-

Read/Write

No